Skip to main content
Associate III
June 27, 2024
Question

Error during debugging in NUCLEO-H743ZI board

Hello,

I am using the STM32H743ZI Nucleo board.

Suddenly The Red LED (Over current LED) is glowing in my Microcontroller. I have checked all the connections properly, and there is no short circuit.

Because of this I can't able to load the Program in it It is showing a Target Not Found Error.

" STMicroelectronics ST-LINK GDB server. Version 7.7.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

Starting server with the following options:

Persistent Mode: Disabled

Logging Level: 1

Listen Port Number: 61235

Status Refresh Delay: 15s

Verbose Mode: Disabled

SWD Debug: Enabled

InitWhile: Enabled

Target no device found

Error in initializing ST-LINK device.

Reason: No device found on target."

When I Checked the Data Sheet. it is written that if the board power consumption in the USB Exceeds 500 mA Then the LED will glow it seems.

I have been powering with my laptop till this morning it was working fine. May I know what is the cause?

Thank you

Regards

Ramachandran S

This topic has been closed for replies.

2 replies

ST Technical Moderator
July 1, 2024

Hello @Ramachandran1992 ,

Maybe you have a wrong power mode setting. Did you change SMPS/LDO settings?

Check with this article the steps on how to recover from such situation : 

https://community.st.com/t5/stm32-mcus/how-to-unbrick-an-stm32h7-after-setting-the-wrong-power-mode/ta-p/49691

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate III
July 5, 2024

hi Imen,

I try all method you suggested, but still now I cannot recover my board to find the target. I don't know what has happened to my board.
thank you

regards

Ramachandran S