Skip to main content
MDupu
Associate
March 26, 2019
Question

Erase memory STM32F415 with STlink/V2

Can I erase memory of STM32F415 using STlink/V2 - but- without the need to connect all 20 Pins required for full development. If yes what Pins are required - can we use Swim (4 pins) only ?

This topic has been closed for replies.

3 replies

Uwe Bonnes
Chief
March 26, 2019

Understand SWD connections. Minimal connections are GND, SWDIO and SWDCLK. Maybe you can use wire jumpers from the STLINK to your target.

MDupu
MDupuAuthor
Associate
March 26, 2019

That's what I thought - but was not sure if this would be supported from the STLink with STM32

S.Ma
Principal
March 26, 2019

yes, these 3 signals should be enough to reflash. unless the code running on the MCU has low power clock stop mode or other things which might make activating the debug mode trickier.