Enabling HS400 on eMMC on STM32H536ZI
Hello,
I am configuring an eMMC 5.1 device on the NUCLEO-H573ZI using the SDMMC1 peripheral. I am trying to understand what the maximum speed mode I can reach with this configuration. I am aware that the eMMC would require a VCCQ that has its own 1.8 V.
I found that the STM32H563 data sheet lists HS200 as supported but HS400 is not supported on the SDMMC peripheral. And the maximum clock in the listed table is 110 MHz at 1.8 V. I was not able to find any HS200/HS400 handling in the HAL.
Can I get confirmation on if HS400 is possible on the board due to the SDMMC limitation? And is HS200 realistically and reasonably achievable with the HAL? Is there any STM32 parts that support HS400?
Thank you.