Skip to main content
SMula
Associate II
September 23, 2019
Question

Does STM32F042K6T6(LQF-32) microcontroller require boot pin to be grounded through resistor?

Hi,

I am working on STM32F042K6T6(LQF-32) ARM microcontroller with STM32CubeMX and Keil software, according to the datasheet boot0 pin is available in pin-31 but when I open the same controller in STM32CubeMX I am neither finding any such pin nor its function like BOOT0

So should I include 10k ohm resistor at pin-31 and ground it irrespective of its availability?

Can anyone help me out here?

Regards

Shivakumar

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
September 23, 2019

Yes, you should have a pull down to ensure consistent start up performance. ​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SMula
SMulaAuthor
Associate II
September 23, 2019

Thank you Clive!

Even though there is no BOOT0 function available in the pin-31(PB8) as attached in the image here, I should directly connect a pull down right?

Otherwise(if I do not use pull down) is there any chances of reading garbage data from stored flash data everytime when I restart the controller?

Regards

Shivakumar

Ozone
Principal
September 23, 2019

> Otherwise(if I do not use pull down) is there any chances of reading garbage data from stored flash data everytime when I restart the controller?

A floating BOOT pin will make your board startup into system mode (ROM bootloader) or other modes seemingly at random.

> Even though there is no BOOT0 function available in the pin-31(PB8) as attached in the image here, I should directly connect a pull down right?

BOOT0 is not "selectable functionality" - it is the pin's functionality at startup (POR), before you application. Check the datasheet.