Skip to main content
NGuig.1
Visitor II
April 17, 2020
Question

Debug problems with STM32CubeIDE with Nucleo-H745ZI-Q

Hello,

I have configuration problem of the STM32CubeIDE debugger with my STM32H7ZI-Q. When I launch the debug it crashes at the adress "0xa05f0000" with SIGTRAP and no more message, I try many things to debug it.

Unfortunately, it shows no results.

No more results ...

I reinstall, the V36 ST-LINK Firmware on :

https://www.st.com/en/development-tools/stsw-link007.html

But this solution doesn't work either and I made a step back now I cannot connect the board as a target. I have this error message "Error in initializing ST-LINK device.

Reason: (4) No device found on target."

So I have two main questions :

  • First how I can fix the damage caused by the last solution ? ( I try to reinstall all the driver but the problems it still here)

  • Then, How can I go through the debug of the IDE for flash and run the program on the board ? What is the setting that I don't see?

Thanks a lot for reading my questions and I hope you could answer they !

This topic has been closed for replies.

1 reply

Curtis B.
Associate III
April 18, 2020

Hi I had ta similar problem with the Nucleo 755 on the M4 core. If I step through the code just behind the semaphore check, then I can press the play button without crashing the debug session.

Regards,

Daniel