Skip to main content
PRedd.111
Associate III
December 22, 2020
Question

Cube ide 1.4 doesn't recognize nucleo 32 board on linux.

I have an STM32 Nucleo 32 (F303K8) and was able to use it before. But 1.4 doesn't seem to recognize the boards. I even connected STLink-v2 device and even that did not get identified.

This topic has been closed for replies.

1 reply

Cartu38 OpenDev
Graduate II
December 22, 2020

Starting STM32CubeIDE 1.4.0 ST-Link server driver is required. Have you installed it ?

Takes care if updating (Thnaks Help>Check for Update) from some release to 1.4.x such drivers are not managed. Only fresh install starting from installer is supporting such.

By the way consider 1.5.1 latest release if possible doing fresh install.