Skip to main content
Associate II
August 6, 2024
Solved

Controlling the brightness of the led using the PWM and optocoupler and 0 -10 volts led driver

I am currently using the STM32F103C8 board, in this, I connect the OPTOCOUPLER  input to the PA6 PIN of stm32 which is the PWM pin, and at the output side I connect the optocoupler's output to the driver's 10v + pin and optocoupler's output with 10v - pin, and I also generate the PWM signal using timer 3 ,and in this i want to control the led brightness using the pwm dutycycle but this is not proper working . give me suggestions what should i do in this case?

 

 

 

this is the pwm initialization code

 

void PWM_Init(void) {
    // Initialization struct
    TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct;
    TIM_OCInitTypeDef TIM_OCInitStruct;
    GPIO_InitTypeDef GPIO_InitStruct;
    
    // Step 1: Initialize TIM3
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
    
    // Configure TIM3 base
    TIM_TimeBaseInitStruct.TIM_Prescaler = 144;
    TIM_TimeBaseInitStruct.TIM_Period = 499;
    TIM_TimeBaseInitStruct.TIM_ClockDivision = TIM_CKD_DIV1;
    TIM_TimeBaseInitStruct.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM3, &TIM_TimeBaseInitStruct);
    TIM_Cmd(TIM3, ENABLE);
    
    // Step 2: Initialize PWM
    TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1;
    TIM_OCInitStruct.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStruct.TIM_OCPolarity = TIM_OCPolarity_Low;
 
    TIM_OCInitStruct.TIM_Pulse = 0;
    
    // Initialize OC1
    TIM_OC1Init(TIM3, &TIM_OCInitStruct);
    TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable);
    
    // Initialize OC2
    TIM_OCInitStruct.TIM_Pulse = 0;
    TIM_OC2Init(TIM3, &TIM_OCInitStruct);
    TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable);
    
    // Initialize OC3
    TIM_OCInitStruct.TIM_Pulse = 0;
    TIM_OC3Init(TIM3, &TIM_OCInitStruct);
    TIM_OC3PreloadConfig(TIM3, TIM_OCPreload_Enable);
 
// Initialize OC4
TIM_OCInitStruct.TIM_Pulse = 0;
    TIM_OC4Init(TIM3, &TIM_OCInitStruct);
    TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable);
    
    // Step 3: Initialize GPIOA (PA6, PA7) and GPIOB (PB0)
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
 
    // Initialize PA6 as push-pull alternate function (PWM output) for LED
    GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
    GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP;
    GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz;
    GPIO_Init(GPIOA, &GPIO_InitStruct);
 
    // Initialize PB0 as push-pull alternate function (PWM output) for LED
    GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP;
    GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz;
    GPIO_Init(GPIOB, &GPIO_InitStruct);
 
}
 
This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 18, 2025

@kunj_2308 wrote:

BLUEPILL board


Hello,

ST resources are only dedicated to supporting genuine ST products. We are not committed to ensuring that clones/fakes products work properly with the firmware we provide.

We suggest to purchase a genuine products and purchase them from known and trusted distributors.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

7 replies

Andrew Neil
Super User
August 6, 2024

Please see the posting tips for how to properly post source code, etc:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 


@kunj_2308 wrote:

I am currently using the STM32F103C8 board


What "STM32F103C8 board" ?

 


@kunj_2308 wrote:

I connect the OPTOCOUPLER 


What optocoupler?

 


@kunj_2308 wrote:

 this is not proper working


What, exactly, does that mean?

So what investigation / testing / debugging have you done to find out what's wrong?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
kunj_2308Author
Associate II
August 6, 2024

okay , thanks for your guidance

BLUEPILL board

optocoupler PC817  

i find that if i give the voltages according to that i am not getting the voltage difference of 10v

Andrew Neil
Super User
August 6, 2024

@kunj_2308 wrote:

okay , thanks for your guidance


See point #3 - provide a schematic of your setup.

Some good, clear photos may also help ...

 


@kunj_2308 wrote:

if i give the voltages according to that i am not getting the voltage difference of 10v


Sorry, I don't understand that.

What voltages? Where? According to what? Difference relative to what?

Again, this would be a lot clearer on a schematic!

 


@kunj_2308 wrote:

optocoupler PC817  


This: https://global.sharp/products/device/lineup/data/pdf/datasheet/PC817XxNSZ1B_e.pdf ?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
August 6, 2024

If you initialize the pin as a GPIO output and toggle it, does it control the LED as expected? If not, there's a hardware issue.

> TIM_OCInitStruct.TIM_Pulse = 0;

This will not produce a PWM signal, but will produce a DC low signal (or high depending on settings).

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
kunj_2308Author
Associate II
August 6, 2024

yes it is toggled

TDK
August 6, 2024

Did you change the TIM_Pulse value to something nonzero? 100 for example.

"If you feel a post has answered your question, please click ""Accept as Solution""."