Skip to main content
Simon Nilsson
Associate
April 2, 2019
Question

Control GPIO of STLINK-V3SET?

  • April 2, 2019
  • 1 reply
  • 1345 views

The product page for  STLINK-V3SET lists the following:

Multi-path bridge USB to SPI/UART/I2C/CAN/GPIOs

I can see in the STM32CubeProgrammer CLI that use can use the SPI/I2C/CAN/UART functions. But can you control the state of the GPIO 0-3 pins in some way?

This topic has been closed for replies.

1 reply

LSimc.1
Associate
March 13, 2023

It would be greatly appreciated if someone could assist with the following matter: I have also been unable to find any references or guides describing the process for controlling the GPIOs of the ST-link V3 using the CLI interface.

Is it even possible?

Thanks