Skip to main content
GDI D.11
Visitor II
February 4, 2020
Question

CONNECTION PIN STM32F030C8

Hello everyone

I'm a novice in the industry. I need to read an STM32F030C8 mounted on a card that does not have the jtag connector and not even connector swd.

However, the card has a personal 10 pin connector connected to the stm32.

I need to know if this chip model can only be read with jtag or also with swd. What are the pins of the stm32f030c8 needed to read it? Which pins of the st link.v2 should they be connected to?

I hope some good soul will help me. Thank you in advance

This topic has been closed for replies.