Skip to main content
damien239955
Visitor II
November 5, 2012
Question

Connecting to the STM32 via an ST-LINKV/2

Posted on November 05, 2012 at 11:30

Hello everyone,

I am currently designing an electronic board with an embedded STM32F217IG on it. I would like to interface my board with my computer through the ST-LINKV/2.

I know it is an on chip debugger but is this component also capable of simply program the STM32 or just doing debugging? It might seem a little dumb but I know some debbugger don't allow the user to flash they just allow to debug and the board stop when you unplug the debugger.

I don't know if I'm clear about what I'm asking?

Also I have another question about the connector on my board. The pin-out of the ST-LINK seems to be a classic JTAG. Am i right?

Thank you by advance for the help

Damien

#stlink #stm32f2-connection
This topic has been closed for replies.

2 replies

frankmeyer9
Associate III
November 5, 2012
Posted on November 05, 2012 at 13:03

I know it is an on chip debugger but is this component also capable of simply program the STM32 or just doing debugging?

 

It can for sure erase/program your custom board.

Saying that, I mean with the help of some PC software, like the ST-Link Utility, or an IDE that supports the ST-Link.

Regarding to the hardware, I would take the Discovery boards as template.

Also I have another question about the connector on my board. The pin-out of the ST-LINK seems to be a classic JTAG. Am i right?

 

Not sure which ST-LINK you mean here.

The separately sold ''ST-Link'' debug adapter is capable of JTAG and SWD.

The builtin variant in the discovery boards is SWD only.

frankmeyer9
Associate III
November 5, 2012
Posted on November 05, 2012 at 13:03

<wonderful forum software crashed again...>