Skip to main content
Associate III
Feb 14, 2026 10:57 AM UTC
Solved

Confirmation Required – Accessories Included with STM32H7B3I-EVAL Board

Respected ST Team,

We are planning to purchase the STM32H7B3I-EVAL evaluation board and would like to confirm the accessories included in the standard package before placing the order. Order link is https://www.st.com/en/evaluation-tools/stm32h7b3i-eval.html?ecmp=tt9470_gl_link_feb2019&rt=db&id=DB4091#documentation

Kindly confirm the following:

  1. Does the board come with a USB programming cable (for the onboard STLINK-V3E) ? If not please share the specification for the same.
  2. Is any external power adapter included with the kit? If not please share the specification for the same. Also share the different combinations to power the board.

  3. Please share the list of accessories included in the package.

  4. Are there any mandatory additional accessories required to use complete feature of the board.

  5. Please share diffrent flashing methods avaible on this evaluation board.

We plan to use this board for development and training purposes, so confirmation of the included items will help us plan the purchase accordingly.

Thank you for your support.

Best regards,
Akademika Lab Solutions

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 14, 2026 12:14 PM UTC

Welcome @vijayajangam, to the community!

  1. No, as stated in UM2662, section 6.1.2 you need a USB Type-A to Micro-B cable. The only restriction is that it must be a cable for data transfer, not one that is only suitable for charging.
  2. No, typically the board is powered via the USB port of Punk 1. However, you can also use a 5V DC adapter, as mentioned in the same UM2662, section 6.3.1.
  3. There is just the board in a bag.
  4. What you want to connect externally depends on the desired application. However, at a minimum, either the above-mentioned USB cable or a 5V power supply is required for power, neither of which are included in the scope of delivery.
  5. A detailed answer to this question would probably go beyond the scope of a thread. However, you have all the options that you also have with the STM32H7B3LIH6QU, which are also listed in AN2606, section 57: i.e. via DFU, FDCAN, I2C, SPI, USARTs, SWD.

Does it answer your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 14, 2026 12:14 PM UTC

Welcome @vijayajangam, to the community!

  1. No, as stated in UM2662, section 6.1.2 you need a USB Type-A to Micro-B cable. The only restriction is that it must be a cable for data transfer, not one that is only suitable for charging.
  2. No, typically the board is powered via the USB port of Punk 1. However, you can also use a 5V DC adapter, as mentioned in the same UM2662, section 6.3.1.
  3. There is just the board in a bag.
  4. What you want to connect externally depends on the desired application. However, at a minimum, either the above-mentioned USB cable or a 5V power supply is required for power, neither of which are included in the scope of delivery.
  5. A detailed answer to this question would probably go beyond the scope of a thread. However, you have all the options that you also have with the STM32H7B3LIH6QU, which are also listed in AN2606, section 57: i.e. via DFU, FDCAN, I2C, SPI, USARTs, SWD.

Does it answer your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
Feb 16, 2026 6:51 AM UTC

Thank You 

Vijaya