Skip to main content
Associate
Feb 14, 2025 1:55 PM UTC
Question

Conecting B-CAMS-OMV with STM32MP257F-EV1

Hi, im planing on running computer vision DL models on multiple STM32 boards. At this moment I will compare a STM32MP256F-EV1 with a STM32H747-DISCO, however i only bought the B-CAMS-OMV and is not the same connector on the MP board. IS there any way o run this camera module on both board, can I just get an adapter from the 30-pin ZIF to the CSI connector?Also i dont is the any suplementary information about the ZIF connector

This topic has been closed for replies.

1 reply

AlexWEI
ST Employee
Oct 11, 2025 3:24 AM UTC

hi

an I just get an adapter from the 30-pin ZIF to the CSI connector?

----you can't do this, for this camera is using RGB signals, the CSI connector is using the mipi-csi signals.