Skip to main content
emil28
Associate III
Apr 25, 2020 7:30 PM UTC
Question

Code works with ST Link V3, but doesn't without

Hello,

I am facing a huge problem for three days, and I don't have any beginning of a solution...

I made a PCB with an STM32L476 and a LoRa chip SX1272. I am using the code given by ST ICube LoraWan. After a join success, I start a custom timer and I send data on my LoRa server. Everything works, I can see the join success and the data on my server, but it works ONLY with the ST Link V3 plugged. It is repeatable, when I unplug the st link V3, sometimes the join request works, sometimes not. Some data are not received, and it looks like the program is blocked.

Maybe I am missing something, an option I need to check...

I am using IAR 8.42.2.

If someone have an idea, because I am completely blocked...

Thanks.

This topic has been closed for replies.