Skip to main content
Associate III
October 20, 2024
Solved

CH2 on ADC1 does not work while CH15 or CH2+CH15 works fine.

  • October 20, 2024
  • 3 replies
  • 2499 views

Hi, I did a code to select which channel I want to enable in operation according to some parameters when I start the ADC configuration and TMR.

I have the ADC2 with ch5 and ch10, this work fine, both channels, or only 1 of them.

On ADC1 I have ch2 and ch15, both work fine, only ch15 also, but only ch2 I'm getting strange values on the buffer, more or less 4 times less than what's supposed to be.

Someone have any idea of what's happening?

Thank you!

 

void start_TMR_ADC_DMA(void){
 // Reinitialize the ADCs to start fresh
 MX_ADC1_Init(); // Reinitialize ADC1
 MX_ADC2_Init(); // Reinitialize ADC2

 ADC_ChannelConfTypeDef sConfig = {0};

 // Variables to count the number of active ADC channels
 uint8_t adc1_num_channels = 0;
 uint8_t adc2_num_channels = 0;

 // Configure ADC1 channels based on global variables
 if (adc1_channel_2 == 1) {
 // Enable ADC1 Channel 2
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig);
 adc1_num_channels++; // Increment channel count
 }

 if (adc1_channel_15 == 1) {
 // Enable ADC1 Channel 15
 sConfig.Channel = ADC_CHANNEL_15;
 sConfig.Rank = (adc1_num_channels == 1) ? ADC_REGULAR_RANK_2 : ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 HAL_ADC_ConfigChannel(&hadc1, &sConfig);
 adc1_num_channels++; // Increment channel count
 }

 // Configure ADC2 channels based on global variables
 if (adc2_channel_5 == 1) {
 // Enable ADC2 Channel 5
 sConfig.Channel = ADC_CHANNEL_5;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 HAL_ADC_ConfigChannel(&hadc2, &sConfig);
 adc2_num_channels++; // Increment channel count
 }

 if (adc2_channel_10 == 1) {
 // Enable ADC2 Channel 10
 sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = (adc2_num_channels == 1) ? ADC_REGULAR_RANK_2 : ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 HAL_ADC_ConfigChannel(&hadc2, &sConfig);
 adc2_num_channels++; // Increment channel count
 }

 // Set the number of conversions based on the number of enabled channels
 if (adc1_num_channels > 0) {
 hadc1.Init.NbrOfConversion = adc1_num_channels;
 if (adc1_num_channels == 1) {
 	hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 } else {
 	hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 }
 HAL_ADC_Init(&hadc1); // Reinitialize ADC1 to apply the new configuration
 }

 if (adc2_num_channels > 0) {
 hadc2.Init.NbrOfConversion = adc2_num_channels;
 if (adc2_num_channels == 1) {
 	hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
 } else {
 	hadc2.Init.ScanConvMode = ADC_SCAN_ENABLE;
 }
 HAL_ADC_Init(&hadc2); // Reinitialize ADC2 to apply the new configuration
 }

 // Reinitialize the timers to start fresh
 MX_TIM2_Init(); // Reinitialize TIM2
 MX_TIM3_Init(); // Reinitialize TIM3

 // Start the ADC DMA for both ADCs, ensuring it starts from the beginning of the buffer
 HAL_ADC_Start_DMA(&hadc1, (uint32_t *)adc_i_buffer, ADC_I_BUF_SIZE); // Start ADC1 DMA
 HAL_ADC_Start_DMA(&hadc2, (uint32_t *)adc_v_buffer, ADC_V_BUF_SIZE); // Start ADC2 DMA with the first buffer

 // Reset buffer loading state
 v_buf_loaded = 0;

 // Start the timers with interrupts
 HAL_TIM_Base_Start_IT(&htim3);
 HAL_TIM_Base_Start_IT(&htim2);
}
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_16B;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 2;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T3_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
 hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc1.Init.OversamplingMode = DISABLE;
 hadc1.Init.Oversampling.Ratio = 1;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
/* sConfig.Channel = ADC_CHANNEL_15;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
/* sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief ADC2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC2_Init(void)
{

 /* USER CODE BEGIN ADC2_Init 0 */

 /* USER CODE END ADC2_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC2_Init 1 */

 /* USER CODE END ADC2_Init 1 */

 /** Common config
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc2.Init.Resolution = ADC_RESOLUTION_16B;
 hadc2.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc2.Init.LowPowerAutoWait = DISABLE;
 hadc2.Init.ContinuousConvMode = DISABLE;
 hadc2.Init.NbrOfConversion = 2;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T3_TRGO;
 hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc2.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
 hadc2.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc2.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc2.Init.OversamplingMode = DISABLE;
 hadc2.Init.Oversampling.Ratio = 1;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
/* sConfig.Channel = ADC_CHANNEL_5;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
/* sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC2_Init 2 */

 /* USER CODE END ADC2_Init 2 */

}

 

This topic has been closed for replies.
Best answer by fposser

My mistake, I change the jumper from SB60 to SB65 and now it's fine.

My jumper configuration of the board was not correct to my usage.

3 replies

STTwo-32
ST Technical Moderator
October 20, 2024

Hello @fposser 

Could you check the errata 2.10.11 of the ES0491. It may be give a discription of the same issue that you are facing.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
fposserAuthor
Associate III
October 20, 2024

I will try to configure my ADC in dual mode to see if it fix the problem:

ADC1 and ADC2 are not impacted when running in dual mode, as they operate sampling and conversion at the same time.

 

And it would not explain why when I select only the CH15 or both it works fine. When I select only Ch2 that I have the wrong value.

Andrew Neil
Super User
October 21, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
fposserAuthor
Associate III
October 21, 2024

This is the NUCLEO-H723ZG.

fposserAuthorBest answer
Associate III
October 23, 2024

My mistake, I change the jumper from SB60 to SB65 and now it's fine.

My jumper configuration of the board was not correct to my usage.