Skip to main content
re.wolff9
Senior
Oct 5, 2021 12:57 PM UTC
Solved

Cannot reflash my STM32G030F

I've designed a board that uses an STM32G030F6 processor.

Now I've updated the software and... (one feature wasn't implemented yet) I cannot connect to the target CPU to flash tne new firmware into the board.

Then you'd think I've programmed the SWD pins to something else that AF1: SWD, but as far as I know: i haven't.

That said, then I should be able to use "connect under reset" and again... that doesn't work. (It should work if I manually hit the reset button, right? )

Both programmers I've tried today program my STM32F072R development board just fine without any trouble.

Any suggestions?

I thought: Maybe there is a way out with the bootloader, but alas, I've not hooked up the "boot0" pin to the programming connector as I usually do... The reason being that by default the 'G030 doesn't have a boot0 pin: that isn't enabled in the default flash config and the pin conflicts with SWD.

I'm a Linux user, don't have access to MS Windows. I use "stlink" software by Texane .

This topic has been closed for replies.
re.wolff9
re.wolff9Best answer
Senior
Oct 5, 2021 5:17 PM UTC

The good news: It suddenly worked. I downloaded my extra feature and it worked first time. Due to high voltages on the board, I prefer not to leave the programmer connected during these tests....

The bad news: I need to go find a windows machine somewhere to upgrade the firmware inside the STLINKs? I'm really not looking forward to that. (Hving to work with windows gives me a headache. Litterally).

2 replies

MM..1
Super User
Oct 5, 2021 1:31 PM UTC

You realy activate SWD UR under reset in Texane_? And maybe your stlink need upgrade fw. I need this when use G chips firstly.

re.wolff9
re.wolff9AuthorBest answer
Senior
Oct 5, 2021 5:17 PM UTC

The good news: It suddenly worked. I downloaded my extra feature and it worked first time. Due to high voltages on the board, I prefer not to leave the programmer connected during these tests....

The bad news: I need to go find a windows machine somewhere to upgrade the firmware inside the STLINKs? I'm really not looking forward to that. (Hving to work with windows gives me a headache. Litterally).