Skip to main content
JFOLE.1
Associate II
June 22, 2020
Question

Cannot connect to STM32L05x MCU with CubeProgrammer and ST-Link V3

Cannot connect to STM32L05x MCU with CubeProgrammer and ST-Link V3 using the CLI with both "connect under reset" and "Normal" modes. However using the same setup I can connect with ST-Link V2.

Is there any reasoning for this?

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
June 22, 2020

Select a slower SWD clock rate, try 1 or 4 MHz rather than 24 MHz

Does your interface connect the NRST pin?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JFOLE.1
JFOLE.1Author
Associate II
June 23, 2020

Yes interface connects to NRST. Clock speed selection doesn't affect it, it will connect in Normal mode but never under reset.

JFOLE.1
JFOLE.1Author
Associate II
July 7, 2020

I have two IC's that I am working with in this project. STM32L07x and STM32L05x.

With STM32L07x I can connect consistently with ST-LINK V2/V3.

However with STM32L05x it is very inconsistent.

I have tried this with numerous samples of each MCU and have concluded that it must be the MCU compatibility.

Another point to note, I can run STM32L07x in both Normal and under reset mode. With STM32L05x I can only use Normal mode, and even with this it can be very inconsistent.

Any ideas?

S.Ma
Principal
July 8, 2020

what voltage the stm32 runs with?

JFOLE.1
JFOLE.1Author
Associate II
July 8, 2020

3.7V at DCDC which then outputs 1.8V to MCU