Skip to main content
FKaes.1
Associate III
Mar 4, 2021 8:14 AM UTC
Solved

Cannot connect STLINK Utility to NUCLEO-L552ZE-Q

Hello, I bought a NUCLEO-L552ZE-Q and tried to connect with STLINK Utility . But STLINK Utility rejects.

08:57:29 : ST-LINK SN : 066CFF505352716587121640
08:57:29 : V2J37M26
08:57:29 : Connected via SWD.
08:57:29 : SWD Frequency = 4,0 MHz.
08:57:29 : Connection mode : Connect Under Reset.
08:57:29 : Debug in Low Power mode enabled.
08:57:29 : Can not connect to the target!
08:57:33 : Unexpected error

I used the lastest ST-LINK Utility v4.6.0.0

Connection other boards, like STM32F4 Disco or STM324R9 Disco worked fine. Therefore STLINK Utility is basicly working

Additional strange is, that the NUCLEO-L552ZE-Q is working fine with CubeID. Programming and debugging is possible.

Therefore, at the moment, only the combination NUCLEO-L552ZE-Q + ST-LINK Utility isn't working.

I used the NUCLEO-L552ZE-Q out of the box. (No jumper modified)

Any ideas ?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Mar 4, 2021 10:01 AM UTC

The ST-Link Utility is a Windows only tool and still active, but the world was requesting tools for all platforms.

With the STM32CubeProgrammer STMicroelectronics therefore provides a multi-platform tool (Windows/Linux/MacOSX) for all recent and newer STM32, which also contains a CLI. You can easily replace the CLI statements in your scripts by the new ones.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
Mar 4, 2021 8:44 AM UTC

Hello @FKaes.1​ ,

Welcome to the STM32 Community :smiling_face_with_smiling_eyes:

Are you able to connect and program it through STM32CubeProgrammer ?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
FKaes.1
FKaes.1Author
Associate III
Mar 4, 2021 9:44 AM UTC

Hello @Imen DAHMEN​ 

>>Are you able to connect and program it through STM32CubeProgrammer ?

yes, I downloaded STM32CubeProgrammer and it is working.

Is ST-Link Utility obsolete ?

Because I'm using ST-LINK CLI in a toolchain and therefore would like to keep it.

I aslo not understand, why only L5 is not working.

 10:30:58 : STM32CubeProgrammer API v 2.6.0
 10:31:11 : ST-LINK SN : 066CFF505352716587121640
 10:31:11 : ST-LINK FW : V2J37M26
 10:31:11 : Board : NUCLEO-L552ZE-Q
 10:31:11 : Voltage : 3.24V
 10:31:11 : SWD freq : 4000 KHz
 10:31:11 : Connect mode: Normal
 10:31:11 : Reset mode : Software reset
 10:31:11 : Device ID : 0x472
 10:31:11 : Revision ID : Rev B
 10:31:12 : UPLOADING OPTION BYTES DATA ...
 10:31:12 : Bank : 0x00
 10:31:12 : Address : 0x40022040
 10:31:12 : Size : 32 Bytes
 10:31:12 : Bank : 0x01
 10:31:12 : Address : 0x40022060
 10:31:12 : Size : 16 Bytes
 10:31:12 : UPLOADING ...
 10:31:12 : Size : 1024 Bytes
 10:31:12 : Address : 0x8000000
 10:31:12 : Read progress:
 10:31:12 : Data read successfully
 10:31:12 : Time elapsed during the read operation is: 00:00:00.009

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Mar 4, 2021 10:01 AM UTC

The ST-Link Utility is a Windows only tool and still active, but the world was requesting tools for all platforms.

With the STM32CubeProgrammer STMicroelectronics therefore provides a multi-platform tool (Windows/Linux/MacOSX) for all recent and newer STM32, which also contains a CLI. You can easily replace the CLI statements in your scripts by the new ones.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
FKaes.1
FKaes.1Author
Associate III
Mar 4, 2021 10:11 AM UTC

Hi @Peter BENSCH​ 

thanks to your answer. I will try to do this.

It would be nice, if STM can add a note at the ST-Link Utility page that is probably fails with new devices and direct to the new tool.

At least, before I created this ticket, I searched the internet and didn't find something to this topic.