Skip to main content
FLast.1
Visitor II
October 18, 2020
Question

Can't connect to target! Two months ago work, now it don't, on two computers windows 8,

There is no fully communication with ST-link V2 with STM32 Link utility program.

All drivers installed properly, signed.

Firmware upgrade mode works, programming mode not.

FW version: V2J33s7

I set low rate speed 100 kHz, try all reset options - never work.

STM target information - detection fail

What I can do now?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
October 18, 2020

Make sure pin 1 or 2 is connected to board supply, and target voltage is reporting correctly.

​

Would need more info on target boards and atta​chment to understand why.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..