Skip to main content
Associate
Oct 1, 2025 8:15 PM UTC
Solved

Can't connect to new board: NUCLEO-N657x0-Q Error: No STM32 target found

Can't connect to new board: NUCLEO-N657x0-Q Error: No STM32 target found

This topic has been closed for replies.
MAK1Best answer
Associate
Oct 2, 2025 11:28 AM UTC

1. Move the JP2 jumper on the NUCLEO-N657x0-Q board to the "top" position.

2. Use the STM32 Programmer v2.20.0 software

3. Set (mouse click on) the connection to "ST-LINK" in the upper right hand ("blue") window of the STMCubeProgrammer software.

4. MOST IMPORTANT: Push the "Reset" button on the lower right corner of the NUCLEO-N657x0-Q board.  (It is to the right of the Ethernet connector - below the LED2, LED3 etc..)

5. Click on "CONNECT" in the upper right hand corner of the STMProgrammer software.

It works!   The STMProgrammer software shows "Connected" and the Log window shows a long message that ends with (2nd to last line) a light green line "Data read successfully"

2 replies

ST Technical Moderator
Oct 1, 2025 9:13 PM UTC

Hello @MAK1 and welcome to the Community,

Please refer to this post that may help you: Solved: Error: No STM32 target found! (SMT32N657X0-Q)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MAK1AuthorBest answer
Associate
Oct 2, 2025 11:28 AM UTC

1. Move the JP2 jumper on the NUCLEO-N657x0-Q board to the "top" position.

2. Use the STM32 Programmer v2.20.0 software

3. Set (mouse click on) the connection to "ST-LINK" in the upper right hand ("blue") window of the STMCubeProgrammer software.

4. MOST IMPORTANT: Push the "Reset" button on the lower right corner of the NUCLEO-N657x0-Q board.  (It is to the right of the Ethernet connector - below the LED2, LED3 etc..)

5. Click on "CONNECT" in the upper right hand corner of the STMProgrammer software.

It works!   The STMProgrammer software shows "Connected" and the Log window shows a long message that ends with (2nd to last line) a light green line "Data read successfully"