Question
Can't auto-start Nucleo-F756 with the external power input
- 1 reply
- 944 views
Hello,
We encountered that Necleo-F756 could not auto-start program with the E5V(+5V), VDD(+12V) external power input.
but it can auto start with USB (ST-Link) power input. I think there is something wrong with the settings. Our setting is below. Could you give me any advice?
[Settings]
1. Power input : +5V => CN11 pin 6 (E5V) , J3 jumper connect between 2 and 1 (E5V) , JP1 no jumper.
2. STM32CubeProbgrammer : check Run after Programing
I attached the Excel file for the details of the Nucleo setting, NRST wave and STM32CubeProgrammer setting.