Skip to main content
Visitor II
Jan 28, 2025 3:56 AM UTC
Solved

Can Nucleo-F446 handle 2 CAN channels simultaneously?

Hi team,

 

I was trying to establish CAN communication between Matlab Simulink and 2 nodes, through STM32 board. Our logic is working fine when checked individual device. But communication is not taking place when respective nodes are connected to Can1 and Can2 and checked parallelly.

 

  1. Is STM32 Nucleo-F446 series board really capable of handling 2 CAN channels simultaneously ?
  2. If no, how can we solve the issue of communicating with both nodes at a time ?

 

Thank you,

M Satya Prashanth

9515992585

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 28, 2025 3:41 PM UTC

Hello @msp171197 and welcome to the community,

First Matlab/Simulink is not the environement developped by ST but it is developed and supported by Mathworks.

So I invite you to submit your request in their community.

Second, I can answer your first question: yes you can use CAN1 and CAN2 simultaneously in both boards: 

Nucleo-F446RE and NUCLEO-F446ZE.But you need to add a CAN transceiver for each CAN instance and establish a complete CAN bus as shown in this figure.

Hope that answers your question.

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 28, 2025 3:41 PM UTC

Hello @msp171197 and welcome to the community,

First Matlab/Simulink is not the environement developped by ST but it is developed and supported by Mathworks.

So I invite you to submit your request in their community.

Second, I can answer your first question: yes you can use CAN1 and CAN2 simultaneously in both boards: 

Nucleo-F446RE and NUCLEO-F446ZE.But you need to add a CAN transceiver for each CAN instance and establish a complete CAN bus as shown in this figure.

Hope that answers your question.

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.