EXT_5V and EXT_3V are internal designations that lead to the network names 5V (P1.1, P1.2) and 3V (P2.1, P2.2) respectively.
Of course, you can also use them as a power supply, but then you should
- check exactly how much current you can draw from the pins of the DISCOVERY, or
- make sure that you stay within the voltage limits when feeding in the corresponding voltage while supplying the DISCOVERY.
Does this answer your question?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.