Skip to main content
ASavi.3
Associate II
May 4, 2022
Solved

Can I program STM32 U585AII6Q with ST-LINK/V2?

I made my own PCB with STM32U585AII6Q and there are pins SWCLK, NRST, SWDIO, GND, VDD which I connected to the ST-LINK/V2. When I try to program STM32 U5, I always have error "No device found on target".

Is there a problem with ST-LINK/V2, do I need to use ST-LINK/V3?

This topic has been closed for replies.
ASavi.3
ASavi.3Best answer
Associate II
May 19, 2022

Thank you!

Everything is fine since I programmed STM32U5 via STM32CubeProgrammer.

3 replies

Mike_ST
ST Technical Moderator
May 4, 2022

Hello,

ST-Link V2 works with STM32U585 too.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
TDK
May 4, 2022

Yes.

Is the board powered? Is a voltage detected in STM32CubeProgrammer?

"If you feel a post has answered your question, please click ""Accept as Solution""."
ASavi.3
ASavi.3AuthorBest answer
Associate II
May 19, 2022

Thank you!

Everything is fine since I programmed STM32U5 via STM32CubeProgrammer.