Skip to main content
CWang.12
Associate II
Jul 29, 2022 8:12 AM UTC
Question

Can I get the reference design about STM32F401X ?

..

This topic has been closed for replies.

4 replies

Andrew Neil
Super User
Jul 29, 2022 8:16 AM UTC

What "reference design", exactly?

Schematics, gerbers, etc, of devboards are on the 'CAD Resources' tab of the board's Product Page

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
CWang.12
CWang.12Author
Associate II
Jul 29, 2022 8:24 AM UTC

Okay, I will look for it .

Andrew Neil
Super User
Jul 29, 2022 8:29 AM UTC

Also look on the chip's Product Page

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
Jul 29, 2022 8:35 AM UTC

Data Sheet and Reference Manual should provide guidance/expectations.

The NUCLEO-F401 might be a good example. Device's pin count my impact specific expectations.

Not many requirements to get functional, need VDD/VDDA, VSS/VSSA, BOOT0 pulled low, bulk capacitance at VCAP pin(s), around 4u7 total, typically split as 2x 2u2, one for each pin, as I recall.

Cap to ground on NRST, also typical, to re-tar-d it's rise.

For programming/debug provide header with VCC,GND,SWDIO,SWCLK,SWO,NRST

A debug/programming UART via USART1 PA9/PA10 recommeded.

Jumper for BOOT0 HIGH/LOW also

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..