Skip to main content
MFord.1
Associate III
June 23, 2020
Question

Can connect to STM32F0 through ST-Link but not through TrueStudio/Debugger.

Hi There,

I have an extremely weird problem.

I have a custom PCB with an STM32F091 chip on it. I am using the SWD interface to connect.

I had another board that is the exact same working and connecting perfectly. I now am trying to get this second board working and I can connect with it through ST-Link utility and I can see on an O-Scope the Reset line being pulled low.

I am getting an error when trying to debug through TrueStudio that it cannot reset the device and on the O-Scope I can see the reset line is not being pulled down. I am completely baffled by this as there is no difference between the two setups and I also had an identical board working and connecting with both.

I have tried rolling back TrueStudio to 9.2 from 9.3 and updating my ST-Link firmware even though it was already up to date.

I am very confused and any ideas would be great!

Thanks

This topic has been closed for replies.