Skip to main content
Associate
Jun 10, 2025 11:52 PM UTC
Solved

CAD resources of NUCLEO-H755ZI-Q Revision D-01

I'm looking for CAD resources of NUCLEO-H755ZI-Q  board Revision D-01. Currently en the web-page there are for revision C-01.

 

Thanks

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
Jul 1, 2025 9:25 AM UTC

Hello,

Update, design files for rev D01 should be there:

CAD resources 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

7 replies

Rodo
Senior
Jun 11, 2025 2:22 AM UTC

It could be that there are no changes to the PCB. You could compare the two BOMs and see what the difference is/are. That would take some time though. It would be nice to have a list of Engineering Change Notices (ECNs) on the schematic or elsewhere.

Mike_ST
ST Technical Moderator
Jun 11, 2025 8:00 AM UTC

Hello,

>> It could be that there are no changes to the PCB

If the revision has moved from C to D, that means PCB has been changed. It could be minor (like silkscreen) or not.

I have entered an internal ticket #211945, to see if it can be added.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Andrew Neil
Super User
Jun 11, 2025 8:35 AM UTC

I see both Revision D-01 and C-01:

AndrewNeil_0-1749630920735.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Mike_ST
ST Technical Moderator
Jun 11, 2025 8:42 AM UTC

>> I see both Revision D-01 and C-01:

Maybe I'm wrong, but I understood the request was for "MB1363 Board design project files" and "MB1363 Manufacturing files" which are only for Rev. C, because, as you mentionned, schematics for rev C and D are there.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Andrew Neil
Super User
Jun 11, 2025 8:51 AM UTC

Maybe:  @Lupillo_1788 just said, "CAD resources" - didn't say what "resources", specifically.

But the BoM, Manufacturing, and Design files are all dated after the D01 schematics ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.