Skip to main content
FJB2069
Senior
Dec 9, 2024 7:59 PM UTC
Solved

Bricked stm32F746-disco with write to Flash?

After testing trying to write a byte to Flash I seemed to have bricked board.  I thought board just went out, so I bought another one, programmed it and now that board is broken too.  I commented code out, tried 3rd board and it works fine.

Here is the code I tried

 

 
uint32_t Flash_Address = 0x80FFF00; 

HAL_FLASH_Unlock();
 FLASH_Erase_Sector(11, FLASH_VOLTAGE_RANGE_2); // Use appropriate sector number and voltage range
 HAL_FLASH_Program(FLASH_TYPEPROGRAM_BYTE, Flash_Address, 0xAA);
 HAL_FLASH_Lock();

 

 

The error I get now is:

Target not halted after reset. Force halt

Failed to halt target

Target not halted

 

Error in initializing ST-LINK device.

Reason: Target not halted.

 

Error in final launch sequence:

 

Failed to execute MI command:

target remote localhost:61234

 

Error message from debugger back end:

localhost:61234: Connection timed out.

Failed to execute MI command:

target remote localhost:61234

 

Error message from debugger back end:

localhost:61234: Connection timed out.

localhost:61234: Connection timed out.

 

I tried using STLINK utility to erase. but they won't connect!

 

Did I use wrong voltage (FLASH_VOLTAGE_RANGE_2)? Not sure if the boards are truly damaged?

 

 

 

 

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 9, 2024 11:54 PM UTC

You're not using a part with 24 sectors

The F746 has 8, describing 1MB

The F767 (24), and F722 (8 for 512KB) might have different array sizes.

As I recollect there are some F4 devices with 2MB, two banks of 1MB in a 16KB*4,64KB*1,128KB*7 pattern

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

6 replies

Tesla DeLorean
Guru
Dec 9, 2024 8:49 PM UTC

That doesn't make a lot of sense. Was there code in that location, or within 128KB? (0x080E0000)

It shouldn't brick the board.

Use STM32 Cube Programmer, or ST-LINK Utilities, try Connect Under Reset, try finding BOOT0 pin/pad and pulling to VDD (HIGH) and connecting that way. When connected, Mass Erase

 

BOOT0 to 3V3, short pads for R42

 

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
FJB2069
FJB2069Author
Senior
Dec 9, 2024 9:47 PM UTC

Yes, that is what I did.  

 

And I wrote to an address to section 7 address 0x0807FF00 without issue.

 

Here is the issue with writing sector 11:  There are only 8 sectors defined in stm32f746xx.h  

/******************************************************************************/
/* */
/* FLASH */
/* */
/******************************************************************************/
/*
* @brief FLASH Total Sectors Number
*/
#define FLASH_SECTOR_TOTAL 8

So how do you access other sectors 9-11?

 

Tesla DeLorean
Guru
Dec 9, 2024 9:57 PM UTC

You're probably thinking of the STM32F4, which had a different mix of different sized sectors.

"On STM32F756xx and STM32F74xx devices, a main memory block divided into 4
sectors of 32 Kbytes, 1 sector of 128 Kbytes and 3 sectors of 256 Kbytes"

Other options on banked devices would be side-to-side (double wide flash lines), or end-to-end

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
FJB2069
FJB2069Author
Senior
Dec 9, 2024 9:29 PM UTC

I was able to recover boards.  Unplug USB, Jumper R42, which is BOOT0 pull up to VCC.  Connect USB, Use st-link to erase.  Unplug USB and remove jumper.  Now you can program as normal.