Skip to main content
Visitor II
August 29, 2023
Question

Boost_VoltageMode_HW example B-G474E-DPOW acts like Buck converter.

  • August 29, 2023
  • 1 reply
  • 883 views

Hello, im wondering if it is some error in name of example, or it is work on purpose?

This topic has been closed for replies.

1 reply

TDK
August 29, 2023
This application runs a Boost converter to output a regulated voltage at 5VDC through two selectable embedded loads.

A Voltage Mode control loop is applied to this Boost plant presuming a 2.5VDC input voltage.
Such input is obtained by halving the 5V provided by USBPD (or alternative user DC supply), through a Buck converter.
Please, note that this Buck converter is used with constant duty cycle (no control loop). 

https://github.com/STMicroelectronics/STM32CubeG4/blob/c4132af65fe74ddd7f54aced85a0f4acce736405/Projects/B-G474E-DPOW1/Applications/Digital_Power/Boost_VoltageMode_HW/readme.txt#L2

It's running both a buck and a boost converter. The example is for the boost portion of this. There are other examples for the buck converter.

"If you feel a post has answered your question, please click ""Accept as Solution""."