Skip to main content
Lalo91
Associate
May 12, 2024
Question

Board to connect webcam and output through HDMI?

  • May 12, 2024
  • 2 replies
  • 1663 views

Hello people.

I just worked on a audio processing project with am STM32F407 discovery board. And everything went fine.

But now I'm looking to work with a board that allows to connect a usb webcam and stream it to 2 monitors through HDMI (I assume this might work better with an MPU rather than an MCU. Since I need the best processing possible on this project.)

The thing is, I have no idea how to pick the right board for this... I don't want to order a bunch of boards and test one by one. I will rather ask to the community for suggestions.

I'd like to mention I'll need the board to have OTG usb, to use it as a host for storing screenshots.

Thanks.

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
May 14, 2024

@Lalo91 wrote:

I assume this might work better with an MPU rather than an MCU. 


Probably.

And, if you're looking for HDMI, probably an SBC rather than a bare MPU.

I'd be looking at something like a Raspberry Pi for this ...

ST's MPU range is here:

https://www.st.com/en/microcontrollers-microprocessors/stm32-arm-cortex-mpus.html

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Lalo91
Lalo91Author
Associate
May 14, 2024

Hello, thanks for your reply back...

I can't fall into SBC's once again, and even less if its por commercial. At first, I built this project in an RPi4 and then migrated it to an Nvidia board... I can't explain enough how much I dislike sbc, since now on, I will work on bare mcu/mpu which at the end is the way to go (harder, but it is), and more if its for commercial.

 

Thanks! I check out the link you provided. I hope to get a "easy" to code board. I wouldn't like to built a library from scratch just you read a webcam and output through hadmi. And actually, not necessarily it needs to be a webcam, I could also look at bare camera modules and connect them directly to gpio.