Question
Best design guidance for an STM32F4 microcontroller operating in both 3.3V & 5V environments?
For long term reliability and not dealing with interface subtleties I practice using 3.3V/5V translators (e.g. SN74LV1T34, ...) rather than taking advantage of the 5 volt tolerant inputs. I see this as reducing the voltage stresses & load current drive, and heating effects to the microcontroller. In a recent design review, a colleague was critical of this approach and thought the design was actually less reliable by adding the translators. What is your opinion?