Skip to main content
hashtala
Associate III
Apr 27, 2020 8:07 PM UTC
Solved

Bare metal STM32F767 MCU programming with ST-Link V2

Hello

I have a question about writing hex file in MCU (STM32F767xx) without a development board.

I want to draw my PCB schematic but I am confused about which pins are used to flash the memory.

I tried finding it on the datasheet but with no luck. Could you please give me directions ?

Also, datasheet claims that on boot-up the MCU uses internal RC oscillator and switches to external one if software commands to. So can I exclude external oscillator and stick with that one only without any major issues ?

This topic has been closed for replies.
Piranha
PiranhaBest answer
Principal III
Apr 27, 2020 8:59 PM UTC

Read AN4661. :)

4 replies

TAndr.1
Associate II
Apr 27, 2020 8:27 PM UTC

If you use SWD then pins SDIO SWCLK and optional SWO for debugging. Internal RC oscillator is less precise then external and more temperature depend.

hashtala
hashtalaAuthor
Associate III
Apr 27, 2020 9:11 PM UTC

OK thanks, got it. I would rather go with external oscillator then

Piranha
PiranhaBest answer
Principal III
Apr 27, 2020 8:59 PM UTC

Read AN4661. :)

hashtala
hashtalaAuthor
Associate III
Apr 27, 2020 9:12 PM UTC

pretty much what I was looking for