Skip to main content
Visitor II
Mar 5, 2026 9:29 AM UTC
Question

B-CAMS-OMV Alternative

Is there any alternative of "B-CAMS-OMV" to use with "STM32F746G-DISCOVERY" as in my region it is not available and the cost will be huge if I want to ship it to Bangladesh. So, is there any alternative modules that I can search for?

2 replies

Peter BENSCH
ST Technical Moderator
Mar 5, 2026 10:21 AM UTC

Welcome @alaraf, to the community!

You could search for:

  1. OV5640 (5Mpx) OMV camera modules (OpenMV-style)

    • same sensor OV5640 as on the B-CAMS-OMV
    • same 1×30 FPC/ZIF OMV form factor
    • typically drop‑in compatible hardware
    • almost unchanged firmware (same I2C address, same register set)

  2. OV2640 (2Mpx) or OV7725 (VGA) OMV camera modules

    • same 1×30 ZIF OMV connector
    • different sensors requiring new init code (different I²C address, register set)
    • DCMI/I²C interface remains the same

Hopefully, your preferred search engine will find suggestions from your region. Just double‑check the 30‑pin OMV pinout (DCMI lines, XCLK, I²C, PWDN, RESET, 3.3V, GND) for mechanical and electrical compatibility.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
EZHON.1
ST Employee
Mar 11, 2026 9:54 AM UTC

can you check if you can order STM32F4DIS-CAM? it may be compatible with the B-CAM-OMV.