Hello @rdevisetti ,
It depends on your needs and what do you plan to evaluate.
- You can consider NUCLEO-F767ZI board for "basic evaluations" it's cheaper than the other boards.
- If you plan to evaluate more advanced features, you can consider STM32F769 Discovery board. For example to use the display / SDcard etc ..
- For more features to access relatively the full MCU features, you can consider STM32F769-EVAL board. For example to use an external NOR FLASH or SRAM via FMC or use CAN etc ..
Refer to the corresponding user manual for each board for more details:
UM1974: STM32 Nucleo-144 boards
UM2033: STM32F769I-DISCO board
UM2035: STM32F769-Eval board
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.