Question
Am working on NUCLEO STM32F401RE , so after debugging the code, am facing this issue. Please advise for this, so i can work speedy. Target no device found Error in initializing ST-LINK device. Reason: No device found on target.
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.