Skip to main content
Visitor II
October 12, 2026
Question

ailed to execute MI command: target remote localhost:61234

  • October 12, 2026
  • 0 replies
  • 4 views
Dear all,
I am using an application on the NUCLEO-F401RE board. I wrote and successfully compiled a program (with no errors), but I am encountering an error during debugging with the message: "Failed to execute MI command: remote target localhost:61234".The ST-LINK (ST-LINK GDB server) is configured as the debug probe and SWD interface.I have replaced the communication cables and reinstalled the STM32CubeIDE software. It used to work normally.
The log is attached below: