Skip to main content
Kura
Associate II
March 11, 2020
Question

About the USB trace impedance needs in device mode

  • March 11, 2020
  • 7 replies
  • 2680 views

I'm referring to USB hardware and PCB guidelines using STM32 MCUs (AN4879)

and to USB 2.0 specification. MCU is STM32H755

In case when Embedded pull-up resistor on USB_DP line, USB 2.0 OTG HS controller with embedded on-chip HS PHYs and mode = device mode:

There (AN4879) were not mentioned about the USB DP or DM impedance or clearance needs, referred only to USB specification. In addition nothing in AN4938. Some manufacturers gives their recommendations to high-speed PCB designs, including USB for some materials. But not found any ST's document about that(?)

  • So the general USB 2.0 high-speed rate differential trace impedance 90 Ω +/- 15% is correct?

I ask because think to need some confirmation before the implementation. Thanks in advance.

This topic has been closed for replies.

7 replies

Singh.Harjit
Senior
March 11, 2020

That is the correct target. The trace width and spacing will be a function of the board's dielectric constant, stack up, and reference plane / trace structure. There are online calculators but those are just an approximation. After you get your boards, think about using a TDR and measuring the traces. You can also ask your board house to do this for you.

Kura
KuraAuthor
Associate II
March 12, 2020

Thanks, I will impelent with 90 Ω. The clearance can be calculated.

K.Ata15
Associate II
March 12, 2020

ST had published some sch and pcb files for older disco/eval boards and if i remember correctly those are impedance matched to 100 mil. As the USB speed is still super slow in newer chips, this should do i guess.

Kura
KuraAuthor
Associate II
March 12, 2020

Actually I have read the schematic of NUCLEO-H743ZI. There were commented the ST-LINK chip USB differential impedance (85-95), and the MCU USB-mode is on that board may dual mode because there is some switch implemented to bus.

The high speed is on H755 is 480 Mb/s, which is the default when microB plug is connected.

But thanks any way.

K.Ata15
Associate II
March 12, 2020

wasn't the internal USB PHY only 12 Mbps, to achieve 480 Mbps you need external chip ?

Kura
KuraAuthor
Associate II
March 12, 2020

.