Skip to main content
KDJEM.1
ST Technical Moderator
May 7, 2026 12:49 PM UTC

STM32H7RS series lifetime usage estimation

This article presents estimated lifetime usage for STM32H7RS series microcontrollers. These estimates are qualified based on the product mission profile, which defines the available lifetime of the product under a specific set of conditions. These conditions include the target junction temperature (TJ), the voltage scaling of the device (VOS), and the duty cycle. The maximum junction temperature (TJmax) and applied voltage values are provided in the product datasheet.

The lifetime estimates in this article are approximate. It must not be considered as an actual lifetime limit or a product guarantee for any single device from the supplier. Applicable sales and warranty terms and conditions remain in effect.

 The table below shows the estimated lifetime usage of STM32H7RS under typical conditions, updated on October 19, 2026.

Note that AN5337, “Guidelines for estimating STM32H7 MCUs lifetime”, is currently applicable for STM32H7RS.

Related links

 

2 replies

Bowman32
ST Employee
Oct 16, 2026 4:50 PM UTC

Application note AN5337 has been updated, and STM32H7RS data has been included. The table in this article should be updated.

KDJEM.1
KDJEM.1Author
ST Technical Moderator
Oct 21, 2026 10:13 AM UTC

Hello ​@Bowman32;

 

Thank you ​@Bowman32 for your comment. The table is updated.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.