Skip to main content
ST Technical Moderator
Apr 17, 2025 1:30 PM UTC

Implementing a USB HID keyboard device from a USB HID mouse application

Summary

This guide helps you migrate an STM32 application from a USB HID mouse to a USB HID keyboard using the STM32 legacy library. Below are the steps to achieve this.

1. Project setup

You can start by obtaining the project from the mouse device project using classic middleware.

Here are the steps:

  1. Start a new project:
    - Open STM32CubeMX.
    - Click [File → New → STM32 Project].
    - Use the [Board Selector] tab and select your board (we use [NUCLEO-C071RB] as an example).
  2. Configure PC13 as user button in EXTI mode.
  3. USB configuration:
    - Enable USB global interrupt
    - Full Speed, using internal PHY and keep other default settings.
    - GPIO Settings: PA11 and PA12 (remapped PA9 and PA10 respectively) as DM and DP.
  4. Copy the necessary library and user files into the project folder. In the following table, you’ll find the necessary middleware files if they don’t already exist:
File name  Source Destination
usbd_core.h Core/Inc CKB-STM32-HID-KEYBOARD-C0/Middlewares/Core/Inc
usbd_ctlreq.h
usbd_ioreq.h
usbd_core.c Core/Src CKB-STM32-HID-KEYBOARD-C0/Middlewares/Core/Src/
usbd_ctlreq.c
usbd_ioreq.c
usbd_hid.h Class/HID CKB-STM32-HID-KEYBOARD-C0/Middlewares/Class/HID
usbd_hid.c

Regarding source files, you can copy following template files and edit them
File name Source Destination
usb_device.h usb_device.h CKB-STM32-HID-KEYBOARD-C0/USB Device/App
usb_device.c usb_device.c
usbd_desc.h usbd_desc.h
usbd_desc.c usbd_desc.c
usbd_conf.h usbd_conf.h CKB-STM32-HID-KEYBOARD-C0/USB Device/Target
usbd_conf.c usbd_conf.c
 

2. Middleware modification

2.1 Update usbd_hid.c

Modify the USBD_HID_CfgDesc in usbd_hid.c to configure it for a keyboard.

Add a macro conditional definition to handle both mouse and keyboard configurations:

__ALIGN_BEGIN static uint8_t USBD_HID_CfgDesc[USB_HID_CONFIG_DESC_SIZ] __ALIGN_END =
{
0x09, /* bLength: Configuration Descriptor size */
USB_DESC_TYPE_CONFIGURATION, /* bDescriptorType: Configuration */
USB_HID_CONFIG_DESC_SIZ, /* wTotalLength: Bytes returned */
0x00,
0x01, /* bNumInterfaces: 1 interface */
0x01, /* bConfigurationValue: Configuration value */
0x00, /* iConfiguration: Index of string descriptor describing the configuration */
#if (USBD_SELF_POWERED == 1U)
0xE0, /* bmAttributes: Bus Powered according to user configuration */
#else
0xA0, /* bmAttributes: Bus Powered according to user configuration */
#endif /* USBD_SELF_POWERED */
USBD_MAX_POWER, /* MaxPower (mA) */

/************** Descriptor of Joystick Mouse interface ****************/
/* 09 */
0x09, /* bLength: Interface Descriptor size */
USB_DESC_TYPE_INTERFACE, /* bDescriptorType: Interface descriptor type */
0x00, /* bInterfaceNumber: Number of Interface */
0x00, /* bAlternateSetting: Alternate setting */
0x01, /* bNumEndpoints */
0x03, /* bInterfaceClass: HID */
0x01, /* bInterfaceSubClass : 1=BOOT, 0=no boot */
#ifdef keyboard 
0x01, /* nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse */
#elif mouse
0x02, /* nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse */
#endif
0, /* iInterface: Index of string descriptor */
/******************** Descriptor of Joystick Mouse HID ********************/
/* 18 */
0x09, /* bLength: HID Descriptor size */
HID_DESCRIPTOR_TYPE, /* bDescriptorType: HID */
0x11, /* bcdHID: HID Class Spec release number */
0x01,
0x00, /* bCountryCode: Hardware target country */
0x01, /* bNumDescriptors: Number of HID class descriptors to follow */
0x22, /* bDescriptorType */
#ifdef keyboard
HID_KEYBOARD_REPORT_DESC_SIZE, /* nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse */
#elif mouse
HID_MOUSE_REPORT_DESC_SIZE, /* wItemLength: Total length of Report descriptor */
#endif
0x00,
/******************** Descriptor of Mouse endpoint ********************/
/* 27 */
0x07, /* bLength: Endpoint Descriptor size */
USB_DESC_TYPE_ENDPOINT, /* bDescriptorType:*/
HID_EPIN_ADDR, /* bEndpointAddress: Endpoint Address (IN) */
0x03, /* bmAttributes: Interrupt endpoint */
HID_EPIN_SIZE, /* wMaxPacketSize: 4 Bytes max */
0x00,
HID_FS_BINTERVAL, /* bInterval: Polling Interval */
/* 34 */
};
#endif

2.2 Define report descriptor size for keyboard in usbd_hid.h

Add the following definitions in usbd_hid.h:

#define HID_MOUSE_REPORT_DESC_SIZE 74U
#define HID_KEYBOARD_REPORT_DESC_SIZE 63U

To complete the implementation of a USB HID keyboard device starting from a USB HID mouse application, follow these steps to update the user application code:

2.3 Define report descriptor for keyboard in usbd_hid.c

To handle the keyboard report descriptor, add the following code snippet in the appropriate section of your middleware files. This defines the HID report descriptor for a keyboard.

#elif keyboard
__ALIGN_BEGIN static uint8_t HID_Keyboard_ReportDesc[HID_KEYBOARD_REPORT_DESC_SIZE] __ALIGN_END =
{
 0x05, 0x01, // USAGE_PAGE (Generic Desktop) 
 0x09, 0x06, // USAGE (Keyboard) 
 0xa1, 0x01, // COLLECTION (Application) 
 0x05, 0x07, // USAGE_PAGE (Keyboard) 
 0x19, 0xe0, // USAGE_MINIMUM (Keyboard LeftControl) 
 0x29, 0xe7, // USAGE_MAXIMUM (Keyboard Right GUI) 
 0x15, 0x00, // LOGICAL_MINIMUM (0) 
 0x25, 0x01, // LOGICAL_MAXIMUM (1) 
 0x75, 0x01, // REPORT_SIZE (1) 
 0x95, 0x08, // REPORT_COUNT (8) 
 0x81, 0x02, // INPUT (Data,Var,Abs) 
 0x95, 0x01, // REPORT_COUNT (1) 
 0x75, 0x08, // REPORT_SIZE (8) 
 0x81, 0x03, // INPUT (Cnst,Var,Abs) 
 0x95, 0x05, // REPORT_COUNT (5) 
 0x75, 0x01, // REPORT_SIZE (1) 
 0x05, 0x08, // USAGE_PAGE (LEDs) 
 0x19, 0x01, // USAGE_MINIMUM (Num Lock) 
 0x29, 0x05, // USAGE_MAXIMUM (Kana) 
 0x91, 0x02, // OUTPUT (Data,Var,Abs) 
 0x95, 0x01, // REPORT_COUNT (1) 
 0x75, 0x03, // REPORT_SIZE (3) 
 0x91, 0x03, // OUTPUT (Cnst,Var,Abs) 
 0x95, 0x06, // REPORT_COUNT (6) 
 0x75, 0x08, // REPORT_SIZE (8) 
 0x15, 0x00, // LOGICAL_MINIMUM (0) 
 0x25, 0x65, // LOGICAL_MAXIMUM (101) 
 0x05, 0x07, // USAGE_PAGE (Keyboard) 
 0x19, 0x00, // USAGE_MINIMUM (Reserved) 
 0x29, 0x65, // USAGE_MAXIMUM (Keyboard Application) 
 0x81, 0x00, // INPUT (Data,Ary,Abs) 
 0xc0 // END_COLLECTION 
};
#endif

This report descriptor defines the structure of data sent and received by the USB HID keyboard. It includes:

  • Modifier keys: Control, Alt, Shift, etc.
  • LED indicators: Num Lock, Caps Lock, etc.
  • Keycode array: For regular key presses.

3. User application code modifications

3.1 Define keyboard data structure and variables

Add the following code in main.c to define the necessary structures and variables for the keyboard:

#ifdef keyboard
extern USBD_HandleTypeDef hUsbDeviceFS;
typedef struct
{
uint8_t MODIFIER;
uint8_t RESERVED;
uint8_t KEYCODE1;
uint8_t KEYCODE2;
uint8_t KEYCODE3;
uint8_t KEYCODE4;
uint8_t KEYCODE5;
uint8_t KEYCODE6;
} keyboardHID;

keyboardHID keyboardhid = {0, 0, 0, 0, 0, 0, 0, 0};
extern uint8_t keyboardpressed;
uint8_t hello_sequence[5] = {0x0B, 0x08, 0x0F, 0x0F, 0x12}; // Keycodes for 'H', 'E', 'L', 'L', 'O'
#endif

3.2 Update usb_device.c

In usb_device.c, after defining extern PCD_HandleTypeDef hpcd_USB_DRD_FS; add the following code to handle keyboard-specific variables:

#ifdef mouse
uint8_t HID_Buffer[4];
#define CURSOR_STEP 5
#elif keyboard
uint8_t keyboardpressed = 0;
#endif

In the same file, update the EXTI interrupt handler to set the keyboardpressed flag when an interrupt is detected and the device is configured:

void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin)
{
 if (GPIO_Pin == BUTTON_USER_Pin)
 {
 if ((((USBD_HandleTypeDef *) hpcd_USB_DRD_FS.pData)->dev_remote_wakeup == 1) &&
 (((USBD_HandleTypeDef *) hpcd_USB_DRD_FS.pData)->dev_state ==
 USBD_STATE_SUSPENDED))
 {
 if ((&hpcd_USB_DRD_FS)->Init.low_power_enable)
 {
 HAL_ResumeTick();
 }
 /* Activate Remote wakeup */
 HAL_PCD_ActivateRemoteWakeup((&hpcd_USB_DRD_FS));

 /* Remote wakeup delay */
 HAL_Delay(10);

 /* Disable Remote wakeup */
 HAL_PCD_DeActivateRemoteWakeup((&hpcd_USB_DRD_FS));

 /* change state to configured */
 ((USBD_HandleTypeDef *) hpcd_USB_DRD_FS.pData)->dev_state = USBD_STATE_CONFIGURED;

 /* Change remote_wakeup feature to 0 */
 ((USBD_HandleTypeDef *) hpcd_USB_DRD_FS.pData)->dev_remote_wakeup = 0;
 remotewakeupon = 1;
 }
 else if (((USBD_HandleTypeDef *) hpcd_USB_DRD_FS.pData)->dev_state ==
 USBD_STATE_CONFIGURED)

#ifdef mouse
 {
 GetPointerData(HID_Buffer);
 USBD_HID_SendReport(&hUsbDeviceFS, HID_Buffer, 4);
 } 
#elif keyboard
 keyboardpressed=1;
#endif 
 }
}

3.3 Main loop

In the main loop, add the following code to handle the keyboard input when the keyboardpressed flag is set:

while (1)
{
/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */
#ifdef keyboard
if (keyboardpressed == 1)
{
for (int i = 0; i < 5; i++)
{
keyboardhid.MODIFIER = 0x00; // No modifier keys
keyboardhid.KEYCODE1 = 0x4E; // Press 'Page Down' button
keyboardhid.KEYCODE2 = hello_sequence[i]; // Press 'H', 'E', 'L', 'L', 'O'
USBD_HID_SendReport(&hUsbDeviceFS, (uint8_t*)&keyboardhid, sizeof(keyboardhid));
HAL_Delay(500);
}
keyboardpressed = 0;
}
else
{
keyboardhid.MODIFIER = 0x00; // No modifier keys
keyboardhid.KEYCODE1 = 0x00; // Release key
keyboardhid.KEYCODE2 = 0x00; // Release key
USBD_HID_SendReport(&hUsbDeviceFS, (uint8_t*)&keyboardhid, sizeof(keyboardhid));
HAL_Delay(500);
}
#endif
}

4. Define predefined symbol in compiler settings

To define the predefined symbol in compiler settings (IAR Workbench is used in our case), follow these steps:

  1. Open [Project Options].
  2. Navigate to [C/C++ Compiler].
  3. Go to [Preprocessor].
  4. In [Defined symbols (one per line)], add the symbol: keyboard.

5. Expected behavior

When opening a text editor, notepad for example, then pressing the USER button on the board, you get the following result as shown in the screenshot below: 

FBL_1-1744713950863.png

Conclusion

By following these steps, you will successfully migrate the user application to implement a USB HID keyboard device starting from a USB HID mouse application.

Related links

2 replies

Associate
Jun 7, 2025 2:54 PM UTC

FBL, your example is very interesting. 

Is it possible to implement both mouse and keyboard with the same usb interface.. I mean that if I press a set of buttons I can move the mouse and if I press another set of button I can send some character as a keyboard. 

Could you suggest some modification to your previous code?

Man

Visitor II
Sep 7, 2025 11:19 PM UTC

Thank you for the nice and clear example. Being relatively new to STM and the CubeIDE, I came here looking for a small USB-Keyboard example.

Trying to reproduce it in the STM32CubeIDE, I ran into a problem with the automatic Code generation (since i'd like to adjust the device configuration later and therefore had to click "Project"|"Generate Code"). I tried two ways:
1) After coping the described files to the respective locations, the "Generate Code" command deleted the created "Middlewares"-folder from my project.
2) Selecting the HID-class from the "Middelwares and Software Packs", "USB_DEVICE" section in the .ioc view, the "Middlewares"-folder remained. But this time, the modifications were removed form the files (usbd_hid.c, usbd_hid.h), once I used the "Generate Code" command.

I tried to protect my code, by putting a self-written "/* USER CODE BEGIN myTest */" and "/* USER CODE END myTest */" around the modification. But this seems to not do the job..

Does anyone have a (hopefully simple?) hint for me. I'd really like to keep to the IDE and not have dig into a whole new toolchain ;)

Kind regards