Skip to main content
ST Employee
May 4, 2023 10:02 AM UTC

How to disable Trustzone on STM32U5 Series

The aim of this article is to provide guidelines for disabling Trustzone on STM32U5.

1. Hardware and software setup

  • Nucleo MB1549-U5A5ZJT6Q1. Hardware and software setup
  • STM32CubeProgrammer

As you can see when connecting your board to STM32CubeProgrammer and checking the option bytes, TZEN is checked (TrustZone® enabled).

1639.png


2. Disable TrustZone®

To disable TrustZone®, you have to:

Step 1: Connect Boot0 to VDD on your board:

This consists on connecting PH3 pin (CN11 pin 7) to VDD (CN11 pin 5).
1640.png

Step 2: Connect your board with STM32CubeProgrammer in "hot plug" Mode.

1641.png


Step 3: Switch RDP value in “readout protection” to level 1, then click on apply.

1642.png

Step 4:

  • Switch RDP value to level 0
  • Uncheck the TZEN value in user configuration. 1643.png

Step 5: Then click on apply to program the option bytes.

1644.png

Step 6: Disconnect your board to STM32CubeProgrammer.
Step 7: Disconnect Boot0 to VDD.
Step 8: Connect again your board with STM32CubeProgrammer and make sure that TrustZone® is disabled(TZEN unchecked). 


1645.png
Reproduce this procedure faithfully otherwise the TrustZone® will not be disabled.

3 replies

Visitor II
Sep 17, 2025 4:03 PM UTC

Hello,
I'm using STM32U385RG in Nucleo-U385RG-Q board. I have been using the trust zone. RDP level was always AA. 

Now I want to disable the trust zone. But I'm stuck at the following error. 
Option Byte Programming failed Or modified by application after OB_LAUNCH

17:59:27 : STM32CubeProgrammer API v2.20.0 | Windows-64Bits
17:59:31 : UR connection mode is defined with the HWrst reset mode
17:59:31 : UR connection mode is defined with the HWrst reset mode
17:59:31 : ST-LINK SN : 002700313234510C33353533
17:59:31 : ST-LINK FW : V3J16M8
17:59:31 : Board : NUCLEO-U385RG-Q
17:59:31 : Voltage : 3.28V
17:59:31 : SWD freq : 8000 KHz
17:59:31 : Connect mode: Hot Plug
17:59:31 : Reset mode : Hardware reset
17:59:31 : Device ID : 0x454
17:59:31 : Revision ID : Rev Z
17:59:31 : Debug in Low Power mode enabled.
17:59:31 : UPLOADING OPTION BYTES DATA ...
17:59:31 : Bank : 0x00
17:59:31 : Address : 0x50022040
17:59:31 : Size : 32 Bytes
17:59:31 : Bank : 0x01
17:59:31 : Address : 0x50022060
17:59:31 : Size : 16 Bytes
17:59:31 : UPLOADING ...
17:59:31 : Size : 1024 Bytes
17:59:31 : Address : 0x8000000
17:59:31 : Read progress:
17:59:31 : Data read successfully
17:59:31 : Time elapsed during the read operation is: 00:00:00.006
18:00:20 : Option byte command : -ob TZEN=0
18:00:20 : qCmd : -ob TZEN=0
18:00:20 : PROGRAMMING OPTION BYTES AREA ...
18:00:20 : Bank : 0x00
18:00:20 : Address : 0x50022040
18:00:20 : Size : 32 Bytes
18:00:21 : Reconnecting...
18:00:26 : Reconnected !
18:00:26 : UPLOADING OPTION BYTES DATA ...
18:00:26 : Bank : 0x00
18:00:26 : Address : 0x50022040
18:00:26 : Size : 32 Bytes
18:00:26 : Bank : 0x01
18:00:26 : Address : 0x50022060
18:00:26 : Size : 16 Bytes
18:00:26 : OPTION BYTE PROGRAMMING VERIFICATION:
18:00:26 : Error: Expected value for Option Byte "TZEN": 0x0, found: 0x1
18:00:26 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
18:00:26 : Time elapsed during option Bytes configuration: 00:00:06.453

Additionally I also tried to erase the full chip flash memory. But I get the same error.

I really appreciate any of your assistance. 

Thanks and regards!

ST Migration account
ST Community Manager
Sep 2, 2026 10:31 AM UTC

I'm also stuck with essentially the same configuration. 

I have a Nucleo-U385RG-Q board. I went straight to trying out the DUA attestation system before flashing any other app. Now I'm stuck with trustzone and intrusion lock, and since there's no "non-secure app" i can boot into, I can't find a way to disable this. 

Did you end up come up with any resolution?

I made a support case but the ST support said they won't help and I should check the community page here.

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
Moktar SELLAMI
ST Employee
Sep 3, 2026 8:57 AM UTC

Hello ​all,  
 

For general information regarding U5/L5 and U3 devices: disabling TZEN can be done during an RDP regression.

There are two ways to disable TrustZone:

  • Via the debug port using STM32CubeProgrammer, as described in the article. The STM32 device should be programmed with an application that includes both secure and non-secure parts.

Having a non-secure application is important because it places the CPU in a non-secure state, which allows the RDP regression to proceed. If the CPU remains in the secure state, the device may interpret the regression as an attack and halt, preventing the RDP regression.

  • Via the system bootloader RSS.

When booting from RSS, the RDP regression may still be possible even if the non-secure application is not running.

We recommend reviewing  the Application note AN5347 section 9.1.2 TZEN/RDP regression with a boot from RSS.

 

If you were unable to boot from RSS and disable TrustZone, please let me know so I can test it on my side and share the following:

  • The Board specific part number 
  • The RSS version  

Other resources:

Best Regards 
Moktar SELLAMI.