FAQ: Using dead battery pins in an STM32 with an integrated UCPD
- 0 replies
- 3487 views
Introduction
Dead battery configuration control (DBCCx) pins play a crucial role in USB Type-C® applications to manage scenarios where the device's main power source is unavailable (dead battery). These pins, used with configuration channel (CC) pins, help the device to be detected and powered by a connected power source. Therefore, this FAQ article covers the dead battery feature whenever it is implemented in an STM32 MCU.

This block resumes the pinout of the UCPD digital controller and the possible connections are detailed in the corresponding datasheet.

1. How should DBCC pins be connected for dead battery support?
For dead battery support, the DBCC pins (UCPDx_DBCC1 and UCPDx_DBCC2) must be externally connected to their respective CC pins (UCPDx_CC1 and UCPDx_CC2). This connection allows the internal pull-down resistor to signal a VBUS supply request when the device is unpowered.
2. What should be done if dead battery support is not required?
If dead battery support is not required (for example, for source-only products), the DBCC pins (UCPDx_DBCC1 and UCPDx_DBCC2) must be tied to ground. This prevents the activation of the internal pull-down resistors, allowing the pins to be used for other functions.
3. How can the dead battery pull-down resistor on UCPD pins be disabled?
The dead battery pull-down resistor on UCPD pins can be disabled by setting the UCPD_DBDIS bit in the PWR_CR3 register for STM32G4 for instance. Dead battery disabling is usually performed by our USB PD stack through HAL_PWREx_DisableUCPDDeadBattery();
This action is performed after the startup sequence, allowing the pins to be used for other functions.
4. What is the internal pull-down resistor value for UCPD pins?
The internal pull-down resistor value for UCPD pins is 5.1kΩ. This ensures that the device can signal a VBUS supply request when unpowered.
5. Can DBCC pins be used as standard GPIOs?
Yes, but these pins have unique characteristics (FT_d or FT_c). When the device is used as a USB Type-C® source or sink without dead battery support, the DBCC pins can be used as GPIOs. You need to ensure that these pins are tied to ground to disable the dead battery pull-down resistors. The design of these IOs is different mainly we have to sustain 5 V when there is no power supply. So, they present more leakage than standard GPIOs.
6. How does UCPD peripheral control Rp and Rd resistors?
UCPD peripheral controls these resistors via ANAMODE and ANASUBMODE[1:0]. Typically, configuration of these registers in handled in USB PD stack. If only one of the CC lines is needed, you can disable control on the other line through the CCENABLE[1:0] bitfield or LL_UCPD_SetccEnable() when initializing cable detection in CAD_Init().
Check coding for ANAMODE, ANASUBMODE, and link with TYPEC_VSTATE_CCx in the corresponding reference manual.
7. What happens when the MCU is unpowered?
When the MCU is unpowered, it still presents the “dead battery” Rd, provided that UCPDx_DBCC1 and UCPDx_DBCC2 pins are each connected to UCPDx_CC1 and UCPDx_CC2 pins, respectively. If dead battery behavior is not required, tie UCPDx_DBCC1 and UCPDx_DBCC2 pins to ground.
8. How should the internal pull-down resistor Rd be managed in different applications?
For applications that do not use the UCPD peripheral, it is recommended to disable the internal pull-down resistor Rd at startup. This is done through the strobe bits in SYSCFG registers as explained in corresponding reference manual.
Applicative use cases
The following section lists the principal topologies of USB Type-C® applications with the dead battery feature as detailed in table 12 in AN5225:
1. VBUS-powered sink example (not protected and supporting dead battery)
- When STM32 MCU is unpowered, Rd is driven by DBCCx (shorted to their respective CCx pins). Upon powering the device, the Rd value transitions to the one defined in the control registers.
2. Sink without dead battery support (not protected and not supporting dead battery)
- The device cannot connect to a source when unpowered. DBCCx pins could be reused for other purposes.
3. Protected sink with dead battery support
- A protection circuit (like TCPP01-M12) is inserted between STM32 pins and CCx pins on the connector. This protection circuit isolates the device's CCx pins from the CCx lines of the Type-C connector.
- When STM32 MCU is unpowered, Rd is driven by TCPP. When VBUS is provided, the TCPP circuit connects the connector pins to STM32 pins.
4. Protected sink without dead battery support:
- Protection circuit is deactivated when supplied.
- Protection circuit is deactivated by software through dedicated input.
- Typically, when unpowered, Rd is controlled by a TCPP protection circuit. When VBUS is provided, TCPP connects the connector pins to STM32 pins.
- Possible hardware implementations:

Use case pros and cons:
| Use case |
Pros |
Cons |
|
1. VBUS-powered sink (dead battery) |
Dead battery support, seamless operation |
Complexity, power consumption |
|
2. Sink without dead battery support |
Simplicity, lower power consumption |
Limited functionality, manual intervention |
|
3. Protected sink with dead battery |
Enhanced protection, dead battery support, seamless transition |
Increased complexity, higher cost |
|
4. Protected sink without dead battery |
Enhanced protection, simplicity |
Limited functionality, manual intervention |
Conclusion
Understanding the proper configuration and management of DBCC pins in USB Type-C® devices is crucial for ensuring seamless power delivery and communication, especially in scenarios where the device's main power source is unavailable.
For further technical specifications, always refer to the corresponding datasheets and reference manuals and check section 11.3.1 DBCC1 and DBCC2 lines in AN5225.
Caution: User should be aware of differences in output timing, speed, and leakage for FT_c FT_d GPIOs compared to standard GPIOs.
Related links
- Application note: Introduction to USB Type-C® Power Delivery for STM32 MCUs and MPUs
- Datasheet: Ultra-low-power Arm® Cortex®-M33 32-bit MCU+TrustZone®+FPU, 240 DMIPS, 4 MB Flash, 2.5 MB SRAM, LTDC, MIPI®DSI, crypto