Skip to main content
ST Technical Moderator
Oct 29, 2024 10:07 AM UTC

FAQ: Possible communication failure between STLINK-V3 and some recent computers

While the STLINK-V3 is compliant with USB 2.0 and exhibits reliable USB performance across various platforms since several years, the USB communication may fail between an STLINK-V3 and some recent computers. 

1. Root cause

The root cause comes from the interoperability issues of a eUSB2 to USB 2.0 High-Speed repeater used on certain recent computers. This repeater doesn’t respect the original USB2 specification. As of September 2024, USB-IF has published a new release of the Embedded USB2 (eUSB2) Physical Layer Supplement to the USB Revision 2.0 Specification (Rev.1.2) on their website. This release now includes a new ECN entitled “Repeater HS SYNC Forward”, addressing the interoperability aspect for future devices.

2. Mitigation

To mitigate potential USB communication failures between your host computer and your STLINK-V3 device (this applies to standalone STLINK-V3SET, STLINK-V3MINIE, STLINK-V3MODS probes, and to embedded STLINK-V3 on Nucleo boards and Discovery kits), we suggest the following tested workarounds:

  1. Try to connect to another USB Type-C® port on your computer if available. Alternatively, using a USB Type-A port of your computer usually solves the issue.
  2. Connect the STLINK-V3 via an external USB High-Speed hub to the USB Type-C® port of your host computer (tested hub reference: Anker332 5in1).
  3. Use a different standalone probe to connect to your target board: ST-LINK/V2, STLINK-V3PWR, Segger J-Link.

Our team is actively exploring additional solutions to this issue. We apologize for any inconvenience this may cause, and we appreciate your understanding as we work to resolve this matter.

 

9 replies

Andrew Neil
Super User
Oct 29, 2024 10:13 AM UTC

In affected cases, would the ST-Link show up in Windows Device Manager (or equivalent on other systems)?

 

Ref: https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MKori.1
Associate III
Nov 18, 2024 4:07 PM UTC

Is the issue with the missing full-speed implementation resolved? Previous it wasn't possible to connect a STLink-V3 via an USB-2 Full-Speed (not High-Speed) Isolator as the driver interface implementation was just an empty shell.


Please also see:
https://community.st.com/t5/stm32-mcus-boards-and-hardware/failed-to-connect-to-stlink-v3-using-a-usb-isolator/m-p/273483/highlight/true#M9452

Explorer
Feb 2, 2025 6:42 PM UTC

This issue also affects any product that uses the STM32F7 for USB 2.0 HS with the built-in PHY (not just STLINK probes).

That means that the STM32F7's USB HS peripheral simply doesn't work with recent Apple Macs. Would love to hear if there's a workaround for this!

FBLAuthor
ST Technical Moderator
Feb 5, 2025 3:40 PM UTC

Hi @davetoaster 

Unfortunately, no software workaround for that interoperability issue with the eUSB repeaters on F7 family.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
Mar 31, 2025 7:45 AM UTC

@davetoaster What I am seeing is that there is some intermittent enumeration on Apple Silicon. M4 Mini back ports are very bad. The front ports are on a hub that works fine though. Laptops you have less choice.

Andrew Neil
Super User
Jun 11, 2025 4:47 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Aug 22, 2025 12:04 PM UTC

Thanks for the hints, I just encountered this issue with STLINK-V3MODS:

  • Device blinks RED LED when USB enumeration problem occurs.
  • Device does not show up in Windows Device Manager.
  • Device may work fine on other machines (i.e. FreeBSD) even VM with windoze on FreeBSD.
  • In my case the cause was USB HUB on the way.
  • Attaching to different USB port directly solved the problem.
Visitor II
Aug 20, 2026 8:14 AM UTC

Any updates on this? We have used and STM32F7 in a device we have on the market, and now are getting a lot of recent reports that users cannot connect it to their computers. The root cause has now been isolated to this issue. Is there a solution in the works?

MSliw.1
Associate
Sep 21, 2026 2:28 PM UTC

STM32C5A3CG nucleo board with STLINK-V3 connects to Macbook Pro M4 only via hub USB 3.0 HS. I tried one cheap 2.0 hub and no success, ST-LINK is visible in some conditions, never it did appear as a device, never was able to reach target MCU.