Skip to main content
This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
November 13, 2024

Hi,

check that your stack size is big enough (the map file should provide some information regarding the stack depth). Try to set 4K for the stack if you do not find information in the map file.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

16 replies

Brian TIDAL
ST Technical Moderator
November 7, 2024

Hi,

the existing demos with  X-NUCLEO-NFC03A1 are ready for NUCLEO-L476RG, NUCLEOF401RE or NUCLEO-F103RB. So some extra effort will be needed to support NUCLEO-G071RB.

  1. download the ST25 embedded NFC library
  2. use STM32CubeMX to generate the initialization of the various interfaces (SPI, LEDs, ST25R95 IRQ_IN and IRQ_OUT) and the main.c skeleton (I've attached the ioc file used on NUCLEO-L476RG, this should help you)
  3. Import the middleware files (rfal_*.c, ndef_*.c from Middlewares/ST/RFAL and Middlewares/ST/NDEF) into your project, import the driver (st25r95*.c from Middlewares/ST/RFAL/st25r95 and logger.c and timer.c from Drivers/BSP/Components)
  4. Import the ndef demo application (ndef_*.c from Common/Src/)
  5. copy the rfal_platform.h from the ndef_rw demo into your project
  6. from main.c provided in the ndef_rw demo, add the missing include files in your main.c and copy from  logUsartInit(&hlogger); up to the end of the while 1 loop

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
November 8, 2024

Hi Brian,

I’ve been trying to implement it directly on my nRF52832 microcontroller, but it’s not working as expected. I followed the steps from your previous reply. Do you have any idea where the issue might be?

The code is provided in the attachments.

Thanks for your help!

Andrew Neil
Super User
November 8, 2024

Have you got it going on one of the ready-to-go demos which @Brian TIDAL listed?

It's always good to have a working reference when porting ...

 


@thompeters2004 wrote:

it’s not working as expected.


So what is it doing ?

How does this differ from what you expected ?

What investigation / testing / debugging have you done to find what's going wrong ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.