Skip to main content
LGrig
Visitor II
February 18, 2019
Solved

X-NUCLEO-NFC03A1 plugged on top of NUCLEO-L476RG example

I am trying to read nfc cards with X-NUCLEO-NFC03A1 plugged on top of NUCLEO-L476RG. However, in the X-CUBE-NFC3 ver. 1.4.0 there is no example for such combination, but according to UM2045 Rev 2 ("The software comes with examples of implementation of such drivers, running on X-NUCLEO-NFC03A1 plugged on top of one NUCLEO-L476RG, NUCLEO-F401RE or NUCLEO-F103RB. ") somewhere should be such an example.

Could you please point out exactly where this example project can be downloaded?

Thanks in advance!

Linards

    This topic has been closed for replies.
    Rene Lenerve
    Rene LenerveBest answer
    ST Employee
    February 18, 2019

    Hi @LGrig​ ,

    Yes you are right, the documentation is indicating the L4 platform, but it is not present in the software package, this is a mistake. Please have a look to the following thread https://community.st.com/s/question/0D50X00009sUl5WSAS/read-the-rfid-of-a-card-with-nfc03a1, I've already made the porting to this platform for someone.

    Let me know if that helps you.

    Regards.

    1 reply

    Rene Lenerve
    Rene LenerveBest answer
    ST Employee
    February 18, 2019

    Hi @LGrig​ ,

    Yes you are right, the documentation is indicating the L4 platform, but it is not present in the software package, this is a mistake. Please have a look to the following thread https://community.st.com/s/question/0D50X00009sUl5WSAS/read-the-rfid-of-a-card-with-nfc03a1, I've already made the porting to this platform for someone.

    Let me know if that helps you.

    Regards.