Skip to main content
Associate III
July 10, 2023
Solved

X-CUBE-NFC6 compilation problem

Compiling X-CUBE-NFC6 related code fails on Linux host. 

To compile code on Linux, the following fix is needed: 

 

 

// rename
#include "st25R3916_irq.h"
// to
#include "st25r3916_irq.h"

 

 

This fix will not affect Windows.

Optionally: rename a file on Linux file system to match include.

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
July 10, 2023

This is indeed a typo in several files nucleo_lxxx_bus.c and should be changed in the next revision. Thank you for pointing this out!

Regards
/Peter

@Brian TIDAL
@Ulysses HERNIOSUS 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
July 10, 2023

This is indeed a typo in several files nucleo_lxxx_bus.c and should be changed in the next revision. Thank you for pointing this out!

Regards
/Peter

@Brian TIDAL
@Ulysses HERNIOSUS 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
July 23, 2023

I was going to make a similar post. Would of saved me a good two hours if I spotted this post earlier. Appreciate your post. thx Lex