Skip to main content
Visitor II
September 16, 2023
Solved

X-CUBE-NFC3 for STM32Cube

I read Getting started with the X-CUBE-NFC3 near field communication transceiver
and I have some questions about the program that runs in the article, how can I successfully get the interface in the demo, is there a more detailed tutorial?

sinuo_0-1694858625796.png

 

    This topic has been closed for replies.
    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    October 10, 2023

    Hi,

    the binary for this demo is inside the X-CUBE-NFC3 package. You just need an X-NUCLEO-NFC03A1 plugged onto a Nucleo board such as NUCLEO-L476RG. Drop the binary into the virtual drive when the board is connected on a PC through the STLink USB. Open a serial terminal over the STLink Virtual Com Port as explained in the UM2045 and you will see the menu .

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    1 reply

    Brian TIDAL
    Brian TIDALBest answer
    ST Technical Moderator
    October 10, 2023

    Hi,

    the binary for this demo is inside the X-CUBE-NFC3 package. You just need an X-NUCLEO-NFC03A1 plugged onto a Nucleo board such as NUCLEO-L476RG. Drop the binary into the virtual drive when the board is connected on a PC through the STLink USB. Open a serial terminal over the STLink Virtual Com Port as explained in the UM2045 and you will see the menu .

    Rgds

    BT

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.