Hi User15749752844702162942,
the maximum sustained read rate that can be achieved with the ST25RU3993 for 96 bit tag EPC length is by using a backscatter link frequency (BLF) of 640 kHz.
- M2 coding --> 600 tag reads/sec
- FM0 coding --> 760 tag reads/sec
The maximum read rate that can be used at full power depends on the country/region and their respective radio regulation laws.
Accounting for a dense reader environment also puts restrictions on the maximum read rate (see channel boundary backscatter).
Cheers,
B