Skip to main content
Mac Nickerson
Associate
Jul 11, 2017 4:56 PM UTC
Solved

What is the Proper Select sequence for ISO14443A with CR95HF?

Posted on July 11, 2017 at 18:56

I am using an arduino using SPI to communicate with a CR95HF.

I can ready the device ID and can detect a Mifare classic card in the RF field.

The problem I have is that I'm unable to select the card and have it respond with the SAK and CRC. All I get is an 87 response from the CR95HF.

Below is the data exchange.

To CR95HF>>>

From CR95HF <<<

>>> 00 04 02 26 07 (Detect card)

<<< 80 05 04 00 28 00 00   (Card response - no collision bit set)

>>> 00 04 03 93 20 08   (start Collision loop to get UID for select)

<<< 80 08 5B 48 66 3F 4A 28 00 00 (card responds with full UID)

>>> 00 04 07 93 70 5B 48 66 3F 08 46 7B (SEL)

<<< 87 00 (timeout?)

What am I missing here?

    This topic has been closed for replies.
    Mac Nickerson
    Mac NickersonBest answer
    Associate
    Jul 12, 2017 6:36 PM UTC
    Posted on July 12, 2017 at 18:36

    The 4A byte is the BCC of the data, so thats required.

    thanks for the help.

    here is the output of my test framework

    >>> 00 04 02 26 07

    <<< 80 05 04 00 28 00 00

    readCard Response: 0x80

    Data Length: 0x5

    <<< 80 05 04 00 28 00 00

    Recieved Card Data:

    7 bytes- 80 05 04 00 28 00 00

    ATQA: 0x4

    Flags: 101000

    Append CRC

    Significant bytes: 8

    Anticollision loop Start

    >>> 00 04 03 93 20 08

    <<< 80 08 5B 48 66 3F 4A 28 00 00

    AntiCol Response: 0x80

    Data Length: 0x08 (8)

    Rcvd: 80 08 5B 48 66 3F 4A 28 00 00

    No more collisions

    Selecting UID: 5B 48 66 3F

    >>> 00 04 08 93 70 5B 48 66 3F 4A 28

    <<< 80 06 08 B6 DD 08 00 00

    AntiCol-SEL Response: 0x80

    Data Length: 0x6

    SAK: 08

    CRC: B6 DD

    <<< 80 06 08 B6 DD 08 00 00

    Anticollision loop End

    AntiCol Data:

    6 bytes- 80 06 08 B6 DD 08

    4 replies

    Peter Boringer
    Visitor II
    Jul 12, 2017 10:03 AM UTC
    Posted on July 12, 2017 at 12:03

    Dear Mac,

    IT seems that the Tag doesn't recognize the command and thus doesn't answer so a timeout at the CR95HF expired.

    Please check your select command, for my understanding the tag on the Req A. command  answer its UID :  

    5B 48 66 3F 4A

    So the sel. command might include it. I suggest to try:

                                       00 04 08 93 70 5B 48 66 3F 4A 28

    CR95 send receive    00 04

    length of data to send         08

    SEL command                         93 70

    UID                                                    5B 48 66 3F 4A

    Transmission flag                                                        28

     Hope it will help

    Regards                                                                                                                                                            

    Mac Nickerson
    Mac NickersonAuthorBest answer
    Associate
    Jul 12, 2017 6:36 PM UTC
    Posted on July 12, 2017 at 18:36

    The 4A byte is the BCC of the data, so thats required.

    thanks for the help.

    here is the output of my test framework

    >>> 00 04 02 26 07

    <<< 80 05 04 00 28 00 00

    readCard Response: 0x80

    Data Length: 0x5

    <<< 80 05 04 00 28 00 00

    Recieved Card Data:

    7 bytes- 80 05 04 00 28 00 00

    ATQA: 0x4

    Flags: 101000

    Append CRC

    Significant bytes: 8

    Anticollision loop Start

    >>> 00 04 03 93 20 08

    <<< 80 08 5B 48 66 3F 4A 28 00 00

    AntiCol Response: 0x80

    Data Length: 0x08 (8)

    Rcvd: 80 08 5B 48 66 3F 4A 28 00 00

    No more collisions

    Selecting UID: 5B 48 66 3F

    >>> 00 04 08 93 70 5B 48 66 3F 4A 28

    <<< 80 06 08 B6 DD 08 00 00

    AntiCol-SEL Response: 0x80

    Data Length: 0x6

    SAK: 08

    CRC: B6 DD

    <<< 80 06 08 B6 DD 08 00 00

    Anticollision loop End

    AntiCol Data:

    6 bytes- 80 06 08 B6 DD 08
    Mac Nickerson
    Associate
    Jul 12, 2017 3:36 PM UTC
    Posted on July 12, 2017 at 17:36

    Thanks, however the UID is only 4 bytes, 5B 48 66 3F. so, I set the response to what you suggested without the 4A and I get the same results.

    Peter Boringer
    Visitor II
    Aug 8, 2018 9:32 AM UTC

    Hello Mac,

    By starting collision loop you will get the UID in 4 bytes + the BCC so you will have to use all those bytes for the sel command but at the end you have to add the CRCA calculation.

    Please try the below command:

    00 04 0A 93 70 5B 48 66 3F 4A DD 13 08 (SEL) same command as

    00 04 08 93 70 5B 48 66 3F 4A 28 but with CRC enabled

    DD13 = CRC A calculation of the command 93 70 5B 48 66 3F 4A

    This should work

    Regards

    PB