Skip to main content
Kris1
Associate II
August 1, 2018
Solved

what is the expected Output at PAOUT pinout of ST25RU3993 UHF Chip.

ST25RU3993 Firmware porting into STM32F407.

Observations, while ST25RU3993 Initialization.

-         Check SPI communication is ok .

-         Check EN pin + SPI communication is ok.

-         Check IRQ Line is ok.

-         Check Crystal is Stable.

-         Check PLL is Locked.

-         ST25RU3993 Initialize() is returns Zero.

                Configuration Parameters of ST25RU3993:

-         Internal Power Amplifier (Init PA).

-         Base Frequency : 867500 (867.5MHz).

-         Reference Clock Frequency : 50 KHz.

                  InventoryGen2() based scanning.

                 ETSI Mode Continuous Modulation is Kept.                    

Observed the Output at the PAOUT as Sequence of Pulses.

Query :

1.      Is Sequence of Pulses are Expected PIE(Pulse Interval Encoding)symbol Output at the PAOUT Pins(PAOUT_P,PAOUT_N).

2.      Can we Observe any Carrier Signal at PAOUT pins(PAOUT_P,PAOUT_N).  

This topic has been closed for replies.
Bart Herse
Bart HerseBest answer
Visitor II
August 23, 2018

HI,

  1. at the PAOUT pins you will see the RF carrier ASK or PR-ASK modulated. The base band data is PIE encoded indeed.
  2. PAOUT_P and PAOUT_N are differential output RF signals which need a matching network so that the output power is 20 dBm. The best point to observe the RF carrier (CW or modulated) with a spectrum analyzer would be right after the BALUN, when the RF signal is single ended referenced to GND.

1 reply

Bart Herse
Bart HerseBest answer
Visitor II
August 23, 2018

HI,

  1. at the PAOUT pins you will see the RF carrier ASK or PR-ASK modulated. The base band data is PIE encoded indeed.
  2. PAOUT_P and PAOUT_N are differential output RF signals which need a matching network so that the output power is 20 dBm. The best point to observe the RF carrier (CW or modulated) with a spectrum analyzer would be right after the BALUN, when the RF signal is single ended referenced to GND.