What does a Security Status = 63 mean when reading a single block from a RFID tag using the ST25R3911B and ISO-15693?
- 1 reply
- 1338 views
Hi,
Hardware Setup: MCU: XMC4200 (infineon) connected to ST25R3911B over SPI, tag is ISO15693 compliant
Software: Using the rfal library and the iso15693 APIs in en.STSW-ST25RFAL001 (V2.1.2)
I am able to successfully read the inventory, write a single block and read a single block from the RFID tag memory.
In my testing, if I write to a single block and read from that same block immediately after (to verify that the write occurred successfully), I get a "Security Stat: 63" on the block read transaction. If I simply read a single block (which is not preceded by a write to the same block the Security Status comes out to be 0)
What does this security status code mean? Why is it not 0?
I have attached the C code snippets for my read_single_block and write_single_block function implementation.
Here is the printout from my Debug UART
******************************************************************
Running Inventory Command
iso15693Inventory status: 0
Found Tag!
ISO15693/NFC-V card found
. UID: E0:08:01:55:AB:75:6C:D5
, DSFID: 0
, RES_FLAG: 0
, CRC: a090
Reading system info
System Info for card with UIDE0:08:01:55:AB:75:6C:D5:
Flags: 0
infoFlags: f
dsfid: 0
afi: 0
numBlocks: 250
blockSize: 8
icReference: 84
Write Contents: 0A, 0C, 41, 47 5F, 39, 35, 37
Iso15693/NFC-V Successful write to block num: 1
Reading block number: 1
Read block 1:
Flags: 0
ErrorCode: 0
SecurityStat: 63
ActualSize: 8
Data: 0A:0C:41:47:5F:39:35:37
Block Num: 1, Read Data Length: 8
Block Contents: 0A, 0C, 41, 47 5F, 39, 35, 37
*************************************************************************