Skip to main content
Ade G.1
Visitor II
June 2, 2020
Solved

What are the 27.12MHz crystal specification for the ST25R3916? The evaluation kit uses Murata XRCGB27M120F3M00R0, which is 30ppm tolerance, 40ppm stability, 6pF load capacitance. Can we use a 100ppm tolerance version, XRCGB27M120F0Z00R0?

..

    This topic has been closed for replies.
    Travis Palmer
    Travis PalmerBest answer
    ST Employee
    June 16, 2020

    Hello,

    the crystal tolerance is mainly given by the standard you want to comply with.

    For ISO14443 it is stated: "The frequency fc of the RF operating field shall be 13,56 MHz ±7 kHz.".

    Which means your crystal frequency drift should not be more then +/-7kHz in total.

    BR Travis

    1 reply

    Travis Palmer
    Travis PalmerBest answer
    ST Employee
    June 16, 2020

    Hello,

    the crystal tolerance is mainly given by the standard you want to comply with.

    For ISO14443 it is stated: "The frequency fc of the RF operating field shall be 13,56 MHz ±7 kHz.".

    Which means your crystal frequency drift should not be more then +/-7kHz in total.

    BR Travis